Date Published:Sep. 06. 2024
Quickly checking the status of machines and equipment visually
There are LED-equipped handles that allow you to check the status of machines and equipment at hand.
By installing the LED illumination linked to the equipment in the worker's line of sight...▶You can check the status of the equipment at hand without having to look up at the signal tower.
Additionally, having the LED in the worker's path is also effective in preventing overlooking the signal tower.
▶By equipping the handle with this function, you can prevent working while the interlock is accidentally released.
The type with a switch allows you to send an electric signal with switch operation, enabling the locking and unlocking of the interlock.(Interlock equipment is required separately.)


Recommended Products
Plastic Handles with LED
Issue/case studies
Safety measures/precautionary measures
Solution samples
Machine Elements