NBK logo

Date Published:Sep. 06. 2024

Moving the control panel of a machine tool horizontally【Workability & Maintenance】

There are units available that rotate the control panel horizontally.

By adjusting the control panel to an easy-to-see angle, work efficiency can be improved.

▶You can pass the control panel wiring through the central hole of the swivel unit.

▶It can be locked at any angle with the attached lever.

Recommended Products

Swivel Mount DKSF



Issue/case studies Installation Method/Maintenance Solution samples Machine Elements