Date Published:Sep. 07. 2021

Auto-Positioning Units Frequently Asked Questions (FAQ)

Contents

Q. How much force is required for rotation?
Q. What voltage is the power supply?
Q. What amperage is the required current?
Q. What is the stop accuracy, more or less?
Q. What motor is used?
Q. Is there a brake function?
Q. How do I check the present position?
Q. Is the present position retained even when the power is turned off?
Q. Is use possible without a transceiver?
Q. Is combined use with a manual handle possible?
Q. What is the wireless communication distance, more or less?
Q. The software (EPU-COM) does not display a communication port.
Q. Is it compliant with dust-proof and waterproof standards?
Q. How do I make a purchase or request an estimate?
Q. Is there a product warranty?

Q. How much force is required for rotation?

The rated torque is 0.8 N・m for EPU-210 and EPU-220 and 0.765 N・m for EPU-100.
For example, 1 kg of force can generate the force required to rotate a handle of about Φ150.

The rated torque can be amplified to 2.7 N・m when using in combination with the high torque adapter EOAT-200-4,
and to 5.4 N・m when with the high torque adapter EOAT-200-8.
*EPU-210 and EPU-220 only. EPU-100 does not support high torque adapters.

Q. What voltage is the power supply?

24 VDC ±10%.

Q. What amperage is the required current?

Maximum 1 A.

Q. What is the stop accuracy, more or less?

±5°.

Q. What motor is used?

A DC geared motor.

Q. Is there a brake function?

The main body has a self-locking mechanism via the gear design.
*EPU-210 and EPU-220 only. For EPU-100, use the optional lock adapter.

Q. How do I check the present position?

The EPU motor has an encoder. It performs a linear conversion of rotation [°] with the feed screw lead [mm] and displays the present position in [mm].

Q. Is the present position retained even when the power is turned off?

The present position is retained as position information in the memory, so when the power is turned off and then on again, the same position information will be used for starting.
Note that if the output shaft is rotated by external force while the power is out, there will be a deviation from the position information retained in the memory, requiring the home position to be redefined.

Q. Is use possible without a transceiver?

EPU-210 can be used without a transceiver.
Also, when using wired connection for EPU-100, direct control via RS-232C is possible from a PC with the dedicated software (EPU-COM) installed.
Other connections require a transceiver.

Q. Is combined use with a manual handle possible?

It is not.
For fine adjustment of the unit, press the JOG movement button on the main body.

Q. What is the wireless communication distance, more or less?

The wireless module reference values are 60 m indoors/1200 m outdoors.
It varies according to the operating environment, due to the influence of obstacles, the surrounding wireless environment, etc.

Q. The software (EPU-COM) does not display a communication port.

Check whether the transceiver driver is installed correctly.
In some cases the transceiver virtual COM port (VCP) driver won’t install unless connected to the Internet.
Download the FTDI VCP driver from the website below and install to the PC.
▶http://www.ftdichip.com/Drivers/VCP.htm

Q. Is it compliant with dust-proof and waterproof standards?

It is compliant with IP65.
*EPU-210 and EPU-220 only. EPU-100 is not compliant with IP standards.

Q. How do I make a purchase or request an estimate?

Contact us as below.

Contact us via telephone
▶+1(484)685-7500
Business hours
8AM to 5PM on weekdays, Eastern Standard Time

Contact us online▶here

Q. Is there a product warranty?

The warranty period for EPU-210, EPU-220, and EPU-100 is 300 hours of operation or one year, whichever is shorter.
The warranty period for the EPC-200-CC, EPC-210-EIP, and EPC-100 transceivers is one year of operation.

Usage Others Food Machinery Medical Equipment FA Devices FA solutions