Ball joint・Angle Hinge
Structure Components
Hexagonpost
Set Collars
Indicators
Scales
Dial
Stages
Ball Rollers (Ball Transfers)
Display Mounting Systems
Swivel Mount
Auto-Positioning Units
Remote Gauge Inspection Cameras
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
SEMI Standard (SEMI S8-0218)Compliant Products
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
Nov. 07. 2023
Jun. 15. 2026
May. 14. 2026
Apr. 27. 2026
Apr. 23. 2026
Nov. 26. 2025
Jun. 28. 2024
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
Jan. 14. 2025
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
Nov. 01. 2024
Key and Their Corresponding KeywaysThis page describes JIS B 1301 "Keys and their corresponding keyways".Jan. 27. 2025 time >
This page describes JIS B 1301 "Keys and their corresponding keyways".
Jan. 27. 2025 time >
Dimensions of Holes for Hexagon Socket Cap ScrewsThis page describes "Dimensions of Holes for Hexagon Socket Cap Screws".Jan. 27. 2025 time >
This page describes "Dimensions of Holes for Hexagon Socket Cap Screws".
What makes our custom screws specialThe machine parts manufacturer Nabeya Bi-tech Kaisha (NBK) at e-nedzi.com manufactures special screws to the customer's specifications, such as tip machining and surface treatment. Special material screws, resin screws and loosening prevention are also available.Jan. 14. 2025 time >
The machine parts manufacturer Nabeya Bi-tech Kaisha (NBK) at e-nedzi.com manufactures special screws to the customer's specifications, such as tip machining and surface treatment. Special material screws, resin screws and loosening prevention are also available.
Jan. 14. 2025 time >
Vol. 13 Explaining the Rust Source "Galvanic Corrosion"Have you ever been surprised by rust suddenly appearing on rust-resistant aluminum? If this happens, the reduced strength resulting from the corrosion brings fears of possible damage. This phenomenon is known as "galvanic corrosion". Today, I will explain this principle and how it can be handled. Jan. 10. 2025 time >
Have you ever been surprised by rust suddenly appearing on rust-resistant aluminum? If this happens, the reduced strength resulting from the corrosion brings fears of possible damage. This phenomenon is known as "galvanic corrosion". Today, I will explain this principle and how it can be handled.
Jan. 10. 2025 time >
Fastening Screws in Areas with Cumulative Pitch Misalignment of Large PanelsDiscover how specially processed screws solved challenges with large equipment panels!Jan. 08. 2025 time >
Discover how specially processed screws solved challenges with large equipment panels!
Jan. 08. 2025 time >
Surface-mount technology (SMT) line width changeover automation cuts workload by about 130 minutes per month.We bring you customer feedback on the handle automation unit they have implemented.Dec. 16. 2024 time >
We bring you customer feedback on the handle automation unit they have implemented.
Dec. 16. 2024 time >
Preventing gaps between the sheet and screw when fastening thin sheetsAre You Facing Issues with Screws Not Fully Tightening When Fixing Thin Plates? NBK's Ultra-Low Profile Hex Socket Head Bolts Are the Solution!Dec. 02. 2024 time >
Are You Facing Issues with Screws Not Fully Tightening When Fixing Thin Plates? NBK's Ultra-Low Profile Hex Socket Head Bolts Are the Solution!
Dec. 02. 2024 time >
What is a Linear Guide Stopper? Introduction to Types and Features!It is a component used to prevent slip-out, falling, and to act as a stopper in case of uncontrolled movement for linear guideways (linear ways, linear guides, slide rails). Nov. 28. 2024 time >
It is a component used to prevent slip-out, falling, and to act as a stopper in case of uncontrolled movement for linear guideways (linear ways, linear guides, slide rails).
Nov. 28. 2024 time >
Line adjustment time for different bottle sizes was reduced by about half.Automation Achieved for Over 20 Manual Adjustments.Customer Testimonials on the Implementation of Auto-Positioning UnitsNov. 27. 2024 time >
Customer Testimonials on the Implementation of Auto-Positioning Units
Nov. 27. 2024 time >
Magnetic shield (permalloy shield) must be fixedScrews for fixing thin plates are available.Nov. 26. 2024 time >
Screws for fixing thin plates are available.
Nov. 26. 2024 time >
Vol.6 Varieties of Screws "Beyond" SUSProbably most of the screws you use are made of either iron or stainless steel. However, there are also screws made from various other materials that possess very interesting characteristics. Perhaps these may be able to resolve some of your problems that you have encountered with iron and stainless steel screws. Today, Nedzigon is here to introduce you to the different types and features of screws made of special materials. Nov. 18. 2024 time >
Probably most of the screws you use are made of either iron or stainless steel. However, there are also screws made from various other materials that possess very interesting characteristics. Perhaps these may be able to resolve some of your problems that you have encountered with iron and stainless steel screws. Today, Nedzigon is here to introduce you to the different types and features of screws made of special materials.
Nov. 18. 2024 time >
Solving common issues with Semiconductor Manufacturing Equipment(Pre-Process)This section introduces countermeasures for the special environments necessary for semiconductor manufacturing equipment (pre-process), and measures to improve productivity.Nov. 18. 2024 time >
This section introduces countermeasures for the special environments necessary for semiconductor manufacturing equipment (pre-process), and measures to improve productivity.
Preventing lever fragments from contaminating food machinery.Introducing plastic levers that are detectable by metal detectors.Nov. 06. 2024 time >
Introducing plastic levers that are detectable by metal detectors.
Nov. 06. 2024 time >
What are clamp levers? Here we explain the characteristics and usage methods that help streamline screw tightening!Description of Machine elements for Designers Clamp Levers Edition page. We introduce here what clamp levers are, the advantages of their use, various usage examples, and their types and characteristics.Nov. 06. 2024 time >
Description of Machine elements for Designers Clamp Levers Edition page. We introduce here what clamp levers are, the advantages of their use, various usage examples, and their types and characteristics.
Why You Should Consider LiLz Battery-Powered Cameras for Equipment Monitoring?The Lilz Gauge Camera is a mountable AI camera that will read any analog gauges or meters, detect blockages, or perform thermal analyses around the facility. It automates any routine manual gauge inspections or facility patrols.Nov. 01. 2024 time >
The Lilz Gauge Camera is a mountable AI camera that will read any analog gauges or meters, detect blockages, or perform thermal analyses around the facility. It automates any routine manual gauge inspections or facility patrols.
Nov. 01. 2024 time >
Chemical Resistance of Chemical-proof ScrewsThis page describes "Chemical Resistance of Chemical-proof Screws" such as ceramic, titanium, resin nickel and Inconel.Oct. 07. 2024 time >
This page describes "Chemical Resistance of Chemical-proof Screws" such as ceramic, titanium, resin nickel and Inconel.
Oct. 07. 2024 time >
NEW SAVE