Date Published:May. 14. 2020
Shaft radial load must be suppressed 【Automation / robots / motorization】
Couplings with constant speed and excellent low-eccentric reaction force should be used
Bar feeder encoder
Miniaturization of the encoder and sensor means that the radial load applied to the shaft increases to the extent of straining the shaft, making suppression of shaft radial load an issue. Bellows couplings can tolerate radial loads and rotate at constant speed even if load on the shaft causes misalignment. Their low eccentric reaction force allows use without impairing encoder and sensor performance.
Recommended product
Issue/case studies
Automation/robots/motorization
Machine Tools
Semiconductor Manufacturing Equipment
Food Machinery
Automotive Manufacturing Process
Medical equipment
FA Devices
Solution samples
Couplings