Date Updated:Apr. 24. 2025
Explanation of Terminology

Explanation of Terminology
Temperature correction factor
This is a factor multiplied to the rated torque and max. torque depending on the operating temperature of Couplicon®.
In XGT2
XGL2
XGS2
XGT-C
XGL-C
XGS-C
MJC
MJS
MJB
MOC
MOR
MOL
MOS
MSF,
the rated torque and max. torque vary.
If ambient
temperature exceeds 30°C, be sure to correct the
rated torque and max. torque with correction factor
shown in the following table.
Ambient temperature | Temperature correction factor |
---|---|
-20℃~30℃ | 1.00 |
30℃~40℃ | 0.80 |
40℃~60℃ | 0.70 |
60℃~120℃ | 0.55 |
MOHS-C MOP-C MSXP-C are superior in heat resistance and the rated torque and max. torque do not vary depending on the operating temperature. Correction by temperature correction factor is not required.
Rotation Diameter
Rotation diameter refers to the larger of the coupling outer diameter (φA) or the diameter with the bolt head protruding (φA1)while rotating.
When using couplings in narrow spaces, pay attention to the rotation diameter. Refer to the table below for rotation diameter details.
The rotation diameter is calculated based on the reference dimensions.
As it fluctuates according to tolerance, build a margin into your design values.

Rotation diameter (by coupling type)
Moment of Inertia
This is a value that indicates the rotational difficulty
of Coupling.
Smaller moment of inertia reduces the load torque at the time of start and stop.
Damping ratio
This is a parameter that represents the damping
property of vibration amplitude.
XGT2
XGL2
XGS2 have a large damping ratio,
thus enabling the servomotor gain to be raised.
>>technical information
Max. rotational frequency
This is a maximum rotational frequency available for Couplicon®.
A value calculated based on peripheral speed 33 m/s is described
and we have confirmed that this frequency does not damage the
unit by a test. (Except for MOM MOHS MKM MWBS )
Max. torque
This is a torque value that can be instantaneously transmitted by Couplicon®.
Allowable operating temperature
This is a temperature available for Couplicon®.
The allowable operating temperature for rubber/
resin-used Couplicon® is as shown in the following
table.
Product Code | Allowable operating temperature |
---|---|
XGT2(O.D. φ56 or Less)/XGL2/XGS2 | -10℃~120℃ |
XGT2(O.D. φ68)/XGT/XGL/XGS |
-20℃~80℃ |
MJC/MJS/MJB | -20℃~60℃ |
MOC/MOR/MOL/MOS | -20℃~80℃ |
MOHS |
-20℃~200℃ |
MOP |
-20℃~120℃ |
MSXP |
-20℃~80℃ |
MSF | -20℃~60℃ |
Thrust Reaction Force
This is a force generated when compressing Couplicon® in the shaft direction.
As the thrust reaction force becomes smaller, the force acting on the motor
also becomes smaller.
Slip Torque
Set screw type couplings directly secure the round shaft using hexagon socket set screws. The slip torque refers to the load torque at which the round shaft begins to slip against the set screws.
Clamping type couplings clamp the round shaft with screw clamping force. The slip torque refers to the load torque at which the round shaft begins to slip against the coupling when tightened with the specified screw tightening torque.
The load torque applied to the coupling must be less than the slip torque. Slip torque varies depending on the operating conditions. Be sure to perform testing under the same conditions as actual use in advance.
Static Torsional Stiffness
This is rigidity against torsion of Couplicon® and the inclination
shown in the graph indicates the static torsional stiffness.
Static torsional stiffness for the entire Couplicon® including
not only deflection part but also hub is described here.
Attachment
There are seven types of shaft attachment methods as follows. Select a method according to your needs.
Set screw type
This is low cost and most common attachment method. However, since the screw point directly contacts the shaft, note that it may damage the shaft or make it difficult to remove the unit.
Clamping type
The bore is contracted by tightening force of the screw to clamp the shaft. Mounting and removal can be easily conducted, which does not damage the shaft.
Split type
the bore portion can be completely divided. Therefore, it can be easily mounted or removed without moving the device. In addition, the shaft is not damaged.
Semi-split type
This is an attachment method in which one side of the hubs is clamping type and the other side is split type. The device can be connected only on the split type side while keeping the clamping type side attached on the shaft.
Key type
As with set screw type, this is a general attachment method and can be applied to the transmission of relatively high torque. To prevent the movement in the shaft direction, this is used together with set screw type and clamping type.
Bushing type
Attachment method using taper wedge effect enables secure and stable attachment. This is suitable to high torque transmission and is the most appropriate for the spindle of a machine tool.
Adapter + Clamping type
This is a type made by inserting an adapter into the clamping type so as to be applied to 1/10 taper shaft of the servomotor.Electrical insulation
This is insulation against electricity between both hubs of Couplicon®.
The electrical insulation value of Couplicon® with rubber/resin
used between both hubs is as shown in the following table.
Product Code | Electric resistance value |
---|---|
XGT2(O.D. φ56 or Less)/XGL2/XGS2 | Not less than 2 MΩ |
XGT2(O.D. φ68)/XGT/XGL/XGS | Not less than 10 kΩ and not more than 1 MΩ |
MJC/MJS/MJB | Not less than 2 MΩ |
MOR/MOL/MOS | Not less than 2 MΩ |
MOHS | Not less than 2 MΩ |
MOP | Not less than 2 MΩ |
MSXP | Not less than 2 MΩ |
MSF | Not less than 2 MΩ |
Constant velocity
This is speed unevenness for one rotation of Couplicon®.
In general, the higher the misalignment is, the lower
the constant velocity becomes.
MFB
MWBS are superior in constant velocity even
when misalignment exists and is appropriate for
detection devices such as encoder.
Backlash
This is a backlash against the rotational direction of Couplicon®.
When high precision positioning is required, select a
Couplicon® with zero backlash.
Eccentric reaction force
This is a force generated when making Couplicon® in eccentric condition.
As the eccentric reaction force becomes smaller, the force acting on the shaft bearing also becomes smaller.
Misalignment
This is a shaft center error.
There are three types of misalignment: eccentricity, argument, and end-play.
For details, please refer to Mounting and Maintenance.