NBK logo

Date Published:May. 10. 2020

Improved coupling insulation properties are required 【Compact / lightweight】

PEEK couplings with good insulation properties should be used

Sputtering equipment

Oldham couplings do not have sufficient insulation, so a larger size is required. PEEK couplings can be used to improve insulation at the same size.

Recommended product

Couplings for Vacuum Variable Capacitor  MSXP-C-W-SP

Issue/case studies Compact/space-saving/lightweight Semiconductor Manufacturing Equipment Medical Equipment FA Devices Solution samples Couplings